This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF5010: 10v, 100mA Precise Reference with REF5010

Part Number: REF5010


Hello,

I have to design a 10v@100mA precise reference with REF5010. But REF5010 can provide only 10mA current. I have modify the circuit for current boost. Simulation are good. Circuit diagram and simulation is also attached. All I need to know is, can REF5010 be operate in mode as shown in circuit diagram(or simulation).

1). Circuit Diagram

2). Simulations in Tina.

REF5010_100mA.TSC

Regards

Zain