Other Parts Discussed in Thread: TPS23861
Hi.
I have a simple circuit connected up exactly as the datasheet shows for a class 3 PD using the TPS2375, it's connected to a PoE switch (TL-SF1008P) which uses the TPS23861. The web site for the PSE product says it's 802.3af compliant however the TPS23861 is 802.3at compliant. I'm having real problems getting the PD to switch on. I've now removed the RDet resistor from the TPS2375 and placed it directly across the two diode bridges in series with a 220 ohm resistor and the PSE is now trying to switch on as it briefly hits 48V and then drops out to detection mode but only when I cut the track to the TPS2375 power rail and the rest of the circuit!! With the 2375 in the circuit all I get is frequent pulses around 5.6V and that's it.
So basically I can only get to a 48V almost working state is by placing the 24.9K + 220Ohm resistor across the HD01 bridge outputs (dual bridges from a H2019 transformer)
Do you know any reason why this is happening and should I be using another TI part as the PD front end instead of the TPS2375? I can't supply schematics as this is plain old school prototyping (so far it's proved to be the quickest route to production!). I've also replaced the 2375 in case I'd shorted out the N/C pin etc and broken it. Any information would be greatly appreciated.
Kind Regards, Dan