This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62067-Q1: Minimum On-time

Part Number: TPS62067-Q1


Dear, Sir.

My customer is considering to apply TPS62067-Q1 as
the switching regulator for VIN=5V, VOUT=1.2V/2A.

The minimum on-time is not defined on the datasheet.
So, I would like to make sure TPS62067-Q1 is no problem
under such VIN & VOUT condition.
Plesae give your advice.

Best Regards,
H. Sakai

  • This configuration is a very typical use condition for this device. It is completely covered by the recommended operating conditions in the datasheet. Figure 11 in the datasheet also shows efficiency data for this condition.