This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: How to use LM3150 to drive 20A output

Part Number: LM3150
Other Parts Discussed in Thread: LM5119

Dear Team,

I would like to know how  can LM3150 drive 20A output?

What's the driver device suit for this application?

Below is the spec:

Vin : 24V or 19V

Vout: 12V, 20A

Thanks

Shaq.

  • Hello Shaquille,

    I do not recommend this device for such a high power output. I recommend that you consider the LM5119 in a dual phase configuration with the outputs tied together. The datasheet goes into detail how to configure the device as described.

    Hope this helps?

    David.