This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD13381F4: Question about mechanical dimensions

Part Number: CSD13381F4


Dear Expert,

Our customer are trying to find the distance and tolerance of the red part in below. 

Could you help us to find it out? Thanks!

Regards,

Ben

  • Ben,

    Thanks for posting

    Using the dimensions on the drawing you can find the spacing
    Gap from center line to middle of solder pad is 0.175 then minus 1/2 the width of the 0.15mm wide solder pad =0.175– (0.15/2 mm)= 0.100 mm

    Then double this to get the total clearance = 0.100 mm x2 = 0.200 mm
    So the dimension you are asking for is 0.2mm.

    Best Regards
    Chris