This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40322: single-output with one-phase design

Part Number: TPS40322


As we want to use TPS40322  as single-output with one-phase. How to deal with the signals of unused channel(BOOT2, CS2, EN2/SS2/GSNS/FB2, HDRV2, ILIM2, LDRV2, PG2, PGND2, SW2)? Just let them unconnected? Or did we need pull-up/down to GND/VCC?

And by the way, in our system, the maximum output current is about 18A, so could one-phase output support this?

Thank you!