Other Parts Discussed in Thread: BQSTUDIO, , BQ76930
I'm able to attach low current loads without an issue, but as soon as I attach my 10A load the DSG bit in operationstatus goes low. I turned off all protections, but there are so many moving parts, maybe I'm missing something? I'll attach a screenshot of the bqstudio registers view when I have the two loads attached (notice that the DSG bit is green for the high current load [fig1] and red for the low current load [fig2]) and I'll attach data memory>settings [fig3] view to show my current settings. Thanks for your help.
Figure 1: High Current Load
Figure 2: Low Current Load
Figure 3: Settings