This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429: Exported schematics doesn't work with EAGLE

Part Number: LM3429


Hello,

I've made some simulations with LM3429 and it worked fine. I had efficiency up to 93% with boost topology :D. But the problem is with exported files. I"ve exported both PCB layout ant schematics. PCB layout works fine with Autodesk Eagle software, but I can't properly open the schematics. After trying to open it, an error appears: 

Error:

line 1, column 35071: redefinition of name 'VDC' in tag <attribute>

LM3429 Schematics.zip

How could I fix this? I'll try to attach zipped schematics.

Thanks in advance

Justinas