Hello,
I am trying to run a webbench thermal simulation of the LM3414 (Vin min is 4.91 V and max is 5.09 V) . My LED (Osram LUW H9GP0) has a forward voltage of 3.45V and a current of 700mA. When I try to make a custom LED in webbench, I get an error that the design cannot be created with the LM3414 since the duty cycle is above the limit.
Webbench calculates the duty cycle to be 102%. Isnt the DC Vled/Vin? So 3.45V/4.91V which is about 70% DC. How is webbench calculating the duty cycle?
Amy