This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61032: Power output issue

Part Number: TPS61032

I followed the typical application schematic in the data sheet.  The output is good.  When I put a resistive load on it, it outputs 5V DC 1.5A continuously, no issue.  When I connect it to an iPhone to charge, the iPhone will seldom start charging (I say seldom because sometimes it does start).  If I hook a un-powered USB hub (with 4 outputs and switches to connect/disconnect each) in-between the boost converter and the iPhone, the phone charges fine.

I was thinking that it may be the speed that the connection is taking place, since it works when there is a push button switch in-between or it may be the output capacitor sizing.

The phone only needs about 0.8A to charge (when it does start).   Please point me in the right direction.