Part Number: REF5030
Hi,
I have the following questions concerning the output capacitor for REF5030. I want to make shure I understand the datasheet (sbos410h, page 21) the right way (language issue).
a) I want to use a ceramic capacitor (10uF) that normally has a very low ESR in the range of 0.015 Ohm. Is the output of the REF5030 stable without a discrete series resistor?
b) If the answer to question a) is "yes", is it better to insert a discrete series resistor (of let's say 1Ohm) to improve noise performance?
Thanks and best regards,
Patrick