Other Parts Discussed in Thread: LM3464
I am using LM3466 to drive 3 strings of LED (350mA each) as per Figure 19 in the data sheet.
Do I have to use a constant current source to drive these application?
I used a bench top DC power supply with current limit setting and found that the LED current is not regulated but continue to climb until reaching the current limit setting of the bench top power supply which is not what I would like to have.
I know the data sheet stated that LM3466 is to use with constant current source but don't understand why.
Does the circuit work properly if I use a constant current source with higher current capability and rely on the LM3466 to regulate the current to desired setting of 350mA for each string?
Best regards,
Chien Nguyen