This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: Conditions / Requirements for Reporting 0% Capacity

Part Number: BQ27421-G1


In Document SLUUAH7B (Quickstart Guide for bq27421-G1), Section 4, paragraph related to TERMINATE VOLTAGE, the text states that the TERMINATE VOLTAGE is the target where the gauge 'typically'  reports 0% capacity.  

What are the other factors that affect the reporting of 0% capacity?  The text of the referenced document notes that the gauge 'learns the level of load spikes' , but does not supply any information of how those are learned or used.  Does the passed charge factor in at all to the 0% reporting condition?  How about ambient or Cell temperature?

We are seeing inconsistent use-times between charge/discharge cycles and wonder if the gauge is indicating 0% capacity when the actual State of Charge condition of the battery may allow continued operation.

I appreciate that the algorithm may be proprietary but as much information that you can provide would be useful.

  • Hi Christoper,
    The videos in the link below would provide further insight on the workings of the algorithm

    www.ti.com/.../support-training.html
    note that the bq27421 uses hardcoded chem ids, so the accuracy expected can't be optimal. For best performance a flash gauge is what you need. The gauge learns delta Voltage if there are current spikes and updates that parameter. That is added to the terminate voltage hence adjusting the point the gauge reports 0.

    thanks
    Onyx