I completed the learning cycle and created the senc file (see attached zip file). But when I program the senc file to battery pack, do CC offset calibration, Board offset calibration, IT enable(0x0021), I found BQ20Z45 can't enter shutdown mode by shutdown command when DSG FET turn on. The battery is unsealed.
Please see my test below.
1. Program the senc file to battery pack, CC offset calibration, Board offset calibration, IT enable(0x0021). CHG and DSG FET are on and current is zero.
2. Send ManufacturerAccess shutdown command, after more than 10s, battery does not enter shutdown mode as expecting. See below test waveform, DSG FET turn off for about 50ms when battery receive shutdown command, then DSG FET turn on again. It's abnormal.
3. Turn off CHG and DSG FET by FETControl (0x46), and send ManufacturerAccess shutdown command, battery enter shutdown mode.
4. Increase Deadband and Charger Present threshold, BQ20Z45 still can't enter shutdown mode by shutdown command when DSG FET turn on.