Hi,
here is a question from customer in RRU application
1. recommended operation condition in datasheet shows Ta spec is -40C to 85C.
2. absolute maximum rating in datasheet shows Tj spec is up to 150C
In customer's application, its board temp is ~95C. So want to check on below:
1. can the part work in above case?
2. if we can secure the Tj to below 150C, can it support long time reliability?
3. many other TI device indicate recommended Tj to be within 125C, is it same for this device?
Thank you