This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: Output accuracy

Part Number: TPS53353

Hello.

Currently we are considering TPS 53353 for the core of the FPGA.

specification

Vin  :12V
Vout:0.9V 15A 0.87Vmin  0.90Vtyp  0.93Vmax
Cout:chemical capacitor 1640uF 5mΩ(820uF 10mΩ×2)
Inductors:0.25uH(2.1mΩ)

In the circuit, the output is thought without using ripple injection circuit using chemical capacitor.
Can you satisfy the output condition at this time?
Also, is there a way if it is not good? (Other devices etc.)

thank you.