This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: Minimum Output capacitor value.

Part Number: TPS53353

Hello,

I designed 12Vin, 1Vout, 15A buck circuit with TPS53353 as attached.

Output capacitor value is recommended 600uF, but it's too high, so wants to know the minimum output capacitor value.

Can I use under 100uF?

Regards,

Nicky

TPS53353_12Vin_1Vout_15A.pdf

  • Nicky,

    Output capacitor selection is a bit complicated. It depends on the type of capacitor (what is the ESR?), switching frequency and your transient load step requirements. I suggest you read the datasheet in detail, especially section 7.4.1. Let me know if you have further questions.