This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: LP8860-Q1 difference of betwin A and B ,C,D version

Part Number: LP8860-Q1

Hi all,

what the different point of LP8860-Q1 family ? there are LP8860AQVFPRQ1,LP8860BQVFPRQ1, C version ......

i can't find it in the datasheet, thanks.

  • Hello,

    Each version of the LP8860_Q1 will have different EEPROM settings such as LED current, switching frequency, number of channels used, max output voltage, etc.. We provide these options so customers can use a version that best matches their application specs, without the need of re-programming. EEPROM settings can still be reconfigured if none of the versions match exactly, but we recommend using one of the pre-existing versions if possible.

    Here is a link to "Selecting the Correct LP8860-Q1 EEPROM Version" app note, which can also be found in the LP8860-Q1 product folder under technical documents. This app note highlights all the details and differences between the available versions.

    www.ti.com/.../snva757c.pdf