Hi team,
My customer is having some questions regarding how to design the SR circuit for UCC28950. The input is universal AC and output is 115V/15.6A.
The questions are:
1. For this application is it better to use full-bridge or center tapped full wave rectifier? What are the difference apart from the peak reverse voltage is doubled for center-tapped full wave rectifier?
2. For 115V output voltage, please recommend what is the suitable Vds rating for SR MOSFET with full-bridge and center tapped full wave rectifier.
3. During the output short condition, would it induce excessive voltage spike on SR FET? Do they need to take this into consideration when picking the SR FET?
4. What is the purpose of output inductor other than filtering? Can they remove output inductor like full-bridge LLC?
Thank you.
Best Regards,
Wei-Hao