This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: VCT never set

Part Number: BQ40Z60

I've attached a log file of a charging sequence (last part). Can someone tell me why the VCT flag is never set? The FC flag is also not set, but I think this is related to the VCT flag. 

Relevant flash settings:

Charging voltage: 4200mV (3S4P pack so total 12600mV)

Charge term taper current : 15mA

Charge term voltage: 75mV 

I think that both of these are reached?

SOC Flag Config A = 0x0C88

SOC Flag Config B = 0x8C

SBS Gauging Configuration[RSOCL] = 1 , in the log file the RSOC reaches 100% this means that VCT does happen?

2.log.zip