This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27201: UCC27201ADDAR input pull down resistor

Part Number: UCC27201


Hi 

Any side effect or limitation if add pull down resistor (2.7kohm) in pin 5 & 6 

thanks a lot 

  • Hi Red,

    Ni hao!

    This is fine as long as the driving stage is able to drive that impedance.

    We also have a 200-kohm pull-down resistor internal on those inputs to keep the driver outputs low if the inputs are allowed to float by the controller:

    Let us know if you have any other questions. If not, please press the Green button for me!!! Xie xie!!!