This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92512: PWM dimming Inductance ring

Part Number: TPS92512


Hi,

There is new project, 24V vin,6 string LED,1.5A,used TPS92512.

Inductance  ring when duty cycle < 100%, 100% duty cycle is OK. PWM frequency is 1Khz. when PWM frequency is 30Khz , the inductance does not ring.  What advice do you have? By the way,  is TPS92512 PWM dimming frequency range 100hz to 1Khz?

  • Hello,

    Do you have scope shots showing what you are talking about? I am not sure I understand what you mean by "inductance ring". Do you have a schematic and BOM I could check as well?

    The 100Hz to 1kHz dimming range is specified only because that is the range where you can get a good dimming ratio. You can dim at higher PWM frequencies, you will just be much more limited in your minimum duty cycle and linear dimming range.

    Regards,

    Clint

  • Hi Clint,

    It can be heard the inductance sound when PWM dimming input duty < 100%,  it is 1Khz frequency sound(PWM dimming is 1Khz).

    PL-Belmon 22 Table-2A-REV2.pdf

  • I see. Audible noise from the inductor is a pretty common issue when PWM dimming in the audible frequency range. This generally requires some experimentation with trying different inductors and/or core technologies until you find one that doesn't exhibit magnetostriction (which causes the audible noise) at the frequency you are using. So it may take a few tries but you can eventually find one that doesn't make noise.

    Regards,

    Clint