This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5175-Q1: DC-DC Boost Converter 12V to 28V at 10A continuous

Part Number: LM5175-Q1
Other Parts Discussed in Thread: TPS40090, LM5175, LM25122-Q1

Tool/software: WEBENCH® Design Tools

Look for an IC Controller for a DC-DC Boost Converter with Input from 10V - 16.5V (nominally 12.3V - 14.5V)  and an Output of 28V (min 24V, max 32V) , 10A continuous current (12A Pk)

While I don't need the Buck portion of this part, Web Bench recommended it but only after I reduced my current requirement to 6A.  I would think the current capability would be dependent on the power FETs that I choose.

Perhaps there is a different Boost only part to consider.  I was also considering the TPS40090/91 part for this project

Thanks in Advance

 Dan Convertino