This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61181: What is the difference between TPS61181A and TPS61181

Part Number: TPS61181

What is the difference between TPS61181A and  TPS61181

  • Hi Stacey,

    The mainly difference is TPS61181A supports 30mA current and TPS61181 supports 25mA. Others are shown as below:

    TPS61181A TPS61181
    CURRENT per channel 30mA 25mA
    Min input voltage 4.5V 5V
    EN and CTRL max voltage rating 20V 7V
    EN and CTRL threshold 2.0V/0.8V 1.2V/0.4V
    EN shutdown delay immediate 32ms