Hi Team
My customer has faced one question.
CH1 is SW waveform,
CH2 is COMP voltage,
CH3 is in current waveform
Vin=12V, Vout=1V to 5V.
Actually we use external Amplfier to to measure Current and Volatge and go back to COM to build Closed loop.
This is for battery testing equipment and need constant Volatge /constant Current (CC/CV control).
Now we face at light load condition. The Inductance current is ship, it also is normaly.
But we found it is not reguar, Maybe there has two continues PWM and next time has three PWM,or onely one PWM.
It is means that it is unstable? Normally it should has one regular PWM even enter into light load mode.
Or maybe noise come from COM pin that result in unregular PWM?
Could you tell me the reason.