Other Parts Discussed in Thread: TINA-TI, , TPS92411
Tool/software: TINA-TI or Spice Models
Hello,
I am a student working on a senior project for an LED company, using the TPS92411 switches and TPS92410 regulator.
I am attempting to run a Cadence PSPICE simulation of the 50W reference design here (http://www.ti.com/lit/ug/tiducu7a/tiducu7a.pdf), and I do not see any switching on the TPS92411 (voltage across is always 0V, so switch never turns off to allow LED current). The gate control on the 92410 is also not the correct rectified sine wave shape. I am getting no errors about models, I am using the transient models from the TI site for each chip. Is there anything obvious I can check or can I send some screenshots so you have a better idea of what I am doing?
Thank you