Other Parts Discussed in Thread: TLC5951
Hi,
Figure 4 in the "TLC6C5712-Q1 Application Reference Guide " shows a minimum "max output current" of 10mA which is set with ref resistor of 61k. I am driving several types of LED some of which require only 2mA to give the required brightness. To achieve the required resolution in dot correction control for these, I really need the max current to be 2mA.
The only way I can see of doing this is to put a shunt resistor in parallel with the LED in order to divert a proportion of the current away from the LED. This works to a degree but I'd like the shunt current to be fixed rather than vary with Voutx. I could I suppose replace the shunt resistor with a discrete current source. Anyway, I'm wondering what thoughts others might have about overcoming this 10mA lower limit.
Thanks,
Paul