Part Number: TPS22916
Hi Sir,
On TPS22916, it have a reverse current protect function when the device is enable.
My question is:
1. if the TPS22916 is disable and Vout have a higher voltage, will there be a current flow from Vout to Vin?
2. If 1 is yes, how many current that will flow from Vout to Vin?
3. if there is 0V on input and 3.8V on the output, will there be a current flow through Vout to Vin?
Thanks,
Patrick