Hi,
I would like to connect the Imon output on the TPS24750 to a ADC input of a microcontroller so that i can monitor the system current consumption. There is not much details on how to do this or specific equations on the datasheet related to this. Can I assume that the current flowing through Rset is going to be equal to the current that will be flowing through Rimon? If this is the case and i assume that the max current flowing though Rset at my set current limit is 0.5mA, then can i scale the output accordingly?
For example, Ioutmax = 360mA will give Current at Rset = 0.5mA, then when Iout = 180mA then current at Rset = 0.25mA?
Thanks