Greetings,
We need a PMIC with following requirements.
1) Input Supply - 12v DC max
2) Output Voltage - 3.3V to 5V (adjustable)
3) Output Current - 2A min
4) Battery will be 1 cell Li-on or LiPo
Currently we are using Bq24295 in one of application problem with that is its 5v o/p viz PMID is connected through FET which sometimes turnoff while switching and thus the controller reboots and creates issue for us.
BQ24250 suits us but its 5v ldo doesnt provides much current to power our core. Our Core has a max consumption of 1.2A on full load. Some other peripherals attached to it increases the consumption to 2A this doesn't includes battery charge current.
We are looking forward for a solution that can also tell us battery potential. Our application is an always running Iot device which requires an power path and battery charger with applicable buck and boost converter.
I hope I have explained everything in understandable way.
Thanks
Aditya Rastogi