Other Parts Discussed in Thread: UCC28063A, UCC28063
Hi,
My customer has the following question:
Can you provide me with any tech notes or TI white papers regarding the SoftStart feature of the PFC controllers UCC2806x?
We are now using the UCC28061, but having trouble after a momentary Vac dropout lasting longer than the 440mSec brown out timer. We put in a soft start circuit that limits the rise slope of the Comp pin and then disconnects after a short time. This circuit gets reset when the auxiliary bias dies but that time is much longer than the few seconds of Vac dropout.
I found app note SLUA587 which tries to do the same thing as we are doing by dragging down the Comp pin for a while but it too suffers from an intelligent way to reset the softstart at a momentary dropout.
The UCC28063A shows some internal chip connections that affect the Comp pin. Do these help the situation we have?
Is the UCC28063A pin-pin compatible to replace the UCC28061 without redoing a major amount of validation testing or pcb layout changes?
Thanks,
Chuchen