on BQ24072RGTR input current (pin 13) set is 1.5Amps, charging current is set to 0.4A.
when i connect a wall adapter which can provide 2A, would the current consumed by the input pin 13 would be 1.5A or roughly 0.4A?. (load is not connected while charging)