This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thermal Information

Other Parts Discussed in Thread: TS5A3159A, HD3SS3212, TS3USB221A, TPS2552D, TPS22961, TPS51225C, TPS63051

Dear sir,

Excuse me. Our customer need to know the thermal information of several devices as below table.

Some data I can find in the datasheet. But empty items I have no idea.

Would you please help to provide them? Thank you very much.

Description

Ta

Tj

Tc

θjc

θja

Pd(W)

TS5A3159ADCKR_SC70-6

-40~85

94.6 during max operation overall 150 max 

88.3 during max operation overall 150 max 

 76.1

259

0.044 @ max I/O current 

TPS2552DRVR_SON6_2X2

-40~85

-40~150

 

85.3

72

1.33

 

 

 

 

 

 

HD3SS3212IRKSR_VQFN20_2P5X4P5

-40~85

 

 

41.8

46.6

 

TS3USB221ARSER_UQFN10_2X1P5

-40~85

 

 

107.9

179.7

 

TPS22961DNYR_WSON8

-40~85

125

 

44.4

44.6

 

TS3A24159DGSR_MSOP10

-40~85

88.0 during max operation overall 150 max

89.4 during max operation overall 150 max 

37.9

154

0.061 @ max I/O current 

TPS51225CRUKR_QFN20_3X3

-40~85

150

 

58.1

94.1

 

INA199A1DCKR

-40~125

150

 

79.5

227.3

 

 

 

 

 

 

 

TPS63051YFFR_DSBGA12

-40~85

-40~150

 

0.7

89.9