Hello
We use the bq20z60R1 V1.05 in our battery design.
During our charging tests in the lower(LTCHG1=1) and higher(HTCHG =1) temperature range we observe that the charge timer doesn't count.
Therefore, no timeout failure occurs in these cases. Is this a bug in this firmware revision V1.05?
The technical reference of the bq20z60 "SLUU386-1" describes the counting of the charge timer as:
Charge Mode Timeout
When Current is ≥ Chg Current Threshold, the bq20z60-R1/bq20z65-R1 starts the Charge Timer. The
Charge Timer is suspended when charge is not active ([LTCHG] = 0, [ST1CHG] = 0, [ST2CHG] = 0, and
[HTCHG] = 0 , or when [DSG] = 1. The Charge Timer is reset when an amount of discharge greater than
Over Charge Recovery is detected or if the pack is removed and reinserted when [NR] = 0. Set Charge
Timeout to 0 to disable this feature.
The bq20z60-R1/bq20z65-R1 goes into charge mode charging timeout if:
• Charge timer ≥ Charge Timeout
In the standard temperature ranges ST1CHG=1 or ST2CHG=1 timeout failure occurs.
The programmed charge current for LTCHG and HTCHG is lower than in the standard temperature ranges.
Regards
Dietmar