This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5V Regulated PSU

Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4

For the below three IC

 Input voltage ( DC ) :- 10V ~ 15V

 I need the

Output voltage ( DC ) :- 4.5V to 5V

 

Output current ( DC )  :- 

 

800mA (TLV1117-50) ,

100mA (UA78L05),

500mA (UA78M05)

 

Please advice if any reference design schematic.