This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: What is the maximum number of DDR4 devices for the current source and sink?

Part Number: TPS51200
Other Parts Discussed in Thread: TPS53317A

Hello,

Can the TPS51200  handle 10 DDR4 devices for current source and sink?

Thank you,

Louie

  • Hello,

    Could you also tell me what the is current for +3.3V power input?

    Thanks in advanced!
    Louie
  • Hi Louie,

    Different DDR4 devices need different VTT current. Please check DDR datasheet or contact DDR manufacturer for the VTT current information.

    TPS51200 is 3A device. To leave margin, I suggest to keep the current below 2A.

    The VIN current of TPS51200  is only a few mA.

    If you want to support 10 DDR4 devices, probably you need a high current device, like TPS53317A. It is a switching converter supporting 6A.

    Thanks

    Qian