This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VAUX4, VPLL, VMMC LDO drop out - can it work from 3.3V where the drop out is spec from 250mV?

Other Parts Discussed in Thread: TPS65930

Hi,

my customer is design IN the TPS65930.

HE would like to use as Vin 3.3V .

however , we notice that VPLL2/1 and VMMC1/2 and VAUX4 require 3.15V where the drop out of the LDO is 250mV at the maximum current.

does these units required the maximum current? if yes , we have a drop out issue, if not, new drop out need to be calculate

in order to check if a drop out of 150mV is OK.

could you tell if Vin of 3.3V is OK when working with these units?

thanks

Amit