This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR23615: DC/DC not working

Part Number: LMR23615


Tool/software: WEBENCH® Design Tools

I have designed a dc/dc based on LMR23615 using the webbench tool 23-26V in 5V/1.5A out. See schematic below. I can measure 4.1V at VCC, I can see some switching at 1.6 MHz at pin 1+2 (see picture below). With RT not connected I have expected 400 kHz. Output voltage is only about 0.82V. I have tested to power the board with 5V after the regulator to check power consumption which is only 100 mA at this point. Any ideas are appreciated.