Hello,
I'm trying to use two TPS61181A to drive one LP097QX1 Display. (12 Strings)
LED-Anode 1 and 2 are presumably connected in the Display Unit.
The Problem I'm facing is that the Lighting works for about 1/2 to 1 Second before turning off.
After turning off, the two Units heat up rapidly.
This happens when Powercycling the Device as well as when disableing, then reenabling them using the EN Pin.
Can somebody explain to me why this is happening and how to fix it?