Other Parts Discussed in Thread: TPS61222, TPS61070
after the suggestion i decided to try TPS61222DCKR.
this booster has a EN pin, which can be used to enable or disable the chip.
here are my test results
1. EN pin is tied low --- vout 2.92V ----- vin 3.3V
2. EN pin tied high ---- vout 5V ---- vin 3.3v
in case one shouldn't the output be zero volt rather then 2.92V.
Thanks