Part Number: LM5175
Hi expert,
I'd like to know the difference between ISNS+/ISNS- current limit and over current limit.
As I know, these tow ways both senses current(input or output / LS-MOSFET ). Cycle-by-cycle current limit will occur when current hit current limit threshold then controller will smaller PWM pulse to limit current. And also we could only sense LS current.
In the other side, average current limit will sense current at input/output to limit. When Iin/Iout hit current limit, controller will discharge SS capacitor. When voltage on SS capacitor is lower than 0.8V, controller will decrease voltage on Vout to limit current. And we could sense current any time.
In conclusion, I have two questions on it,
- Why we need to apply two ways for current limit? Or what situation will apply two current limit way in same application?
- If we want to apply two ways in one application, how can we set current limit on it? For example, 6V~24V->12V/5A, OCP=5.5A.
Thank you!
Best regards,
Ann Lien