Other Parts Discussed in Thread: TPS3620, TPS3619
I don't know if my google foo is failing, but does TI have anything similar to the MAX690T?
I need to switch in a battery backup if the AC line goes away.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Keith,
If you are looking for 3.3V monitoring, TPS3606 should work. This has all of the features plus a few additional features. http://www.ti.com/lit/ds/symlink/tps3606-33.pdf
If you don't need the watchdog feature, TPS3619 and TPS3620 will be ideal. http://www.ti.com/lit/ds/symlink/tps3620.pdf
If 5V monitoring will work, TPS3617 will work. http://www.ti.com/lit/ds/symlink/tps3617-50.pdf
To see all of our devices with battery back-up feature:
Please let me know if you have any questions or need any support. Thanks!
-Michael