Part Number: TPS61165
I am testing a device that requires this chip in order to drive an LED backlight. The TPS61165 has been failing during ESD testing. The failure occurs during air discharge testing. I am looking for a good way to protect this device from the ESD discharges since this device is part of the test setup, not the device we are trying to test. I have tried using inductance in the LED connections, but this does not allow the circuit to work. I added a 24V TVS diode to the LED output, but this also failed.