A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ25703Ai want to make 5v output dc voltage with battery backup 7.4 v lithium ion 2 cell 3000 mAh so please suggest use of which ic is required for that.
When the 5V input source is removed, do you allow the 5V output having a glitch ( drops to zero temporary)? If the system allow the 5V output having a glitch, you can pick BQ25703A. When 5V input source is removed, the host controller enables the BQ25703A's OTG function.