This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BTP Output Pin never clears after being set

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50

Hi,

I have a similar problem as .

That thread wasn't answered.
The only difference is that I use BQ40Z50-R1. Once BTP_INT is set, it can be cleared only by device reset, which is unacceptable for me.
I have updated the firmware to bq40z50_r1_ v1.06_build_36, but the problem persisted.
Is there any way to get this feature working right (i.e. set when the remaining capacity has depleted to a certain level, and clear when it is above this level)?


Best regards, Michael.