Other Parts Discussed in Thread: TIDA-00668,
we are using Li-poly battery with below specs.
max voltage : 4.35V
discharge cutoff voltage : 3V
we are thinking to incorporate inductive charging into the device. I have read the datasheet and also Qi spec V1.2.
based on Qi wireless power consortium spec, 5W receiver coil should be L = 1.5.3uH or L = 23.8uH.
my question is, can i design the coil on rigid PCB board?