Hello,
Regarding to 100% Duty-Cycle Operation on TLV62130, my customer is asking some question.
(Question)
(1) According to formula(3) on datasheet page11, the minimum input voltage is following.
VIN(min) = VOUT(min) + IOUT(RDS(on) +RL )
For example, VOUT(min)=3.8V, Iout=.1.1A, Rds(on) =0.09 ohm, inductor(22uH) DCR=0.035ohm -> VIN(min)=3.93V
In this case, when input is less than 3.93V (< 3.93V), device become to 100% Duty-Cycle Operation mode.
My understanding is correct?
(2) In case of the input voltage is crossed to output voltage (Normal Operation <-> 100% Duty-Cycle Operation),
Is there any possible problem on output ? (For example, output accuracy ,regulation )
Or is there other possible problem?
(3) Do you have some information of 100% Duty-Cycle Operation more detail?
(Application Note.)
Regards,
Tao2199