This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: QMAX and OCV Taken not getting set after discharge

Part Number: BQ34Z100-G1

Hi,

We are using a BQ34z100-G1 chip in my application.

We have previously qualified the battery as a CHEM ID 0808, max deviation 11.04% using the GPCTools.

After a successful charge cycle we have performed a discharge cycle at aprox C/5 rate.

ISSUE: After a long relax time, OCVTAKEN did not update. Consequently, we do not get a valid SOH update.

This same situation has occurred on other cycles and other batteries we have tested.

Can you please examine the attached log file and gg.csv file and provide and provide an explanation?

Thank you in advance!bat12 cycle (05-03-2018).zip

Attached is the gg.csv file and data log.