Other Parts Discussed in Thread: BQ24103, BQ25703A, BQ25600, BQ24715, BQ24650, BQ25703
For our battery charger, we are considering some part such as bq24103, which we have used on a different project. I wonder how well this interacts with a solar panel input.
According to the data sheet, when the charger is in CC (constant current) mode, it will demand a fixed current determined by the setting, such as 1.5A. Now if the solar cannot provide 1.5A, then I would expect the voltage on the solar panel will collapse below the battery voltage, at which point the charger will enter a sleep-state. This will allow the panel to re-establish some voltage, but then the charger will turn back on and demand 1.5A again, in a cycle.
However, we actually tried the experiment and found that if the panel can only deliver a small current, such as 100mA, then the system will settle into a steady state where the charger is delivering 100mA to the battery, (which is in fact a desired behavior). This doesn’t seem to be documented by the datasheet, so is there an explanation for it ? Would this be typical of all similar chargers with integrated DC/DC, or will this behavior depend on the charger, and in that case, how can we know the behavior in advance from the datasheet ?
Thanks - Gil