This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A-Q1: ESD improvement

Part Number: BQ76PL455A-Q1

Can we add other ESD device? How to do it?

  • Mr. Hu,

    refer to the table 6.2 for ESD rating of the each of the pins.

    each of the sense inputs is protected (differentially) by the ESD structures with max rating of 6.5V.

    refer to  SLUA791... The reference schematics gives the TVS( Z1 @88V)-FIG Fig 2 and Fig3... scheme to protect the entire modules. also

    refer to the scheme of the protecting the sense lines with zener clamps as in Fig 7.

    Hope this helps.